Other Parts Discussed in Thread: ISO1212, TIDA-01508, ISO1211, TIDA-010049, TIDA-00017, SN65HVS882, SN65HVS885, TPS272C45, TIDA-01552, TPS274160, TIOS101
Hello,
I'm writing this message because I haven't found something very convenient, hope your advice will help !
I'm currently looking to an interface IC for a PLC application with Digital Input and Digital Output capabilities. In my dream, SPI interface is available with the possibility to configure the N ports of the IC as a Digital Input Type 1, 2 or 3 or as a Digital Output. Power supply is 24V. I do not need isolation (I can arrange this in the design at the SPI level).
I found a concurrent device at Maxim Integrated (MAX14906), and I'm looking for alternative to compare several references.
Thanks for the experience feedback !
Regards,
Joel