Part Number: DS92LX1621
Hello Support team
I want to check the transmission quality of a signal pattern that is difficult to transmit with DS92LX162x.
What is the input test pattern for DIN[13:0], HSYNC, VSYNC that meets the following criteria?
- PCLK: 10MHz
- DOUT signal run length : 27
EX) DIN[13:0] = 01 1001 1111 1001, HSYNC = 1, VSYNC = 0
Best Regards,
Hirokazu Takahashi