Other Parts Discussed in Thread: DS90LV031A, DS90LV032A, CDCLVD2106, SN65LVDS108
I have few questions:
- Is there a naming convention related to ANSI TIA/EIA-644-A and ANSI TIA/EIA-644 compatibility? For example, DS90LV031a, DS90LV032a Transmit and Receive pair are ANSI TIA/EIA-644 Standard compatible, DS90LT011AQ, DS90LT012ATLD Transmit and Receive pair are ANSI TIA/EIA-644-A Standard compatible.
- Is there a special meaning between LV and LT?
- We need a 6 channel LVDS Buffer. I can only find CDCLVD2106 which operates at 2.5V. Is there a 3.3V version?