Part Number: DS25BR120
Hi,
Recently I download DS25BR120 ibis model. In this model missing AMI,DLL files. I need those details. please share those details
Example :
IBIS-AMI models consist of three main components:
- Analog models for the transmitter (Tx) and receiver (Rx) to be used for generating a channel response required by the AMI DLL. This analog model is usually a legacy .ibs file containing [Model](s) for the Tx and Rx buffers, and under each of these [Model] statements a keyword [Algorithmic Model] which references the .ami and the .dll executable(s).
- Algorithmic models (the DLL executables) contain signal processing algorithms, not circuit descriptions. These are usually compiled for the Windows and Linux 32 and 64 bit Operating Systems.
- A parameter file (.ami) for each of the algorithmic models.
You must have all three of these files for each buffer to have a complete solution.
The analog models are used to characterize the channel and generate an impulse response, which is a fundamental input for the algorithmic models (the .dll). In the example below, the [Model] section describes the analog model portion of an RX IBIS-AMI model.