Part Number: TCAN1043-Q1
Hello,
My customer is looking for alternative device of NXP TJA1043TK.
PKG is VSON.
I have TI TCAN1043XXX-Q1 device inventory having device top marking as follows.
Is this device P2P compatible with NXP TJA1043TK?
TJA1043TK's max. data rate spec. is 5Mbps.
My customer would like to know item no.detail(XXXX) by top making in advance.
add G suffix:corespond to 5Mbps(specially I would like to know......)
add H suffix:corespond bus fault protection voltage +/-70V

| order no. | MOQ | bus fault protection | max data rate | devide marking | PKG |
| TCAN1043GDMTRQ1 | 3000 | ±58V | 5Mbps | 1043 | VSON |
| TCAN1043GDMTTQ1 | 250 | ±58V | 5Mbps | 1043 | VSON |
| TCAN1043HGDMTRQ1 | 3000 | ±70V | 5Mbps | 1043 | VSON |
| TCAN1043HGDMTTQ1 | 250 | ±70V | 5Mbps | 1043 | VSON |
| TCAN1043DMTRQ1 | 3000 | ±58V | 2Mbps | 1043 | VSON |
| TCAN1043DMTTQ1 | 250 | ±58V | 2Mbps | 1043 | VSON |
| TCAN1043HDMTRQ1 | 3000 | ±70V | 2Mbps | 1043 | VSON |
| TCAN1043HDMTTQ1 | 250 | ±70V | 2Mbps | 1043 | VSON |
| TJA1043TK | 6000 | N/A | 5Mbps | JA1043 | VSON |
Could you please tell identification method from top marking?
Best regards,
ken