Part Number: XIO2001
Hello,
I have about 10 PCI cards, (based on xio2001),some working properly and some not working. From the measurements I made, I see that in those who do not work, the voltage VDD_15_COMB starts at 1.5 V, rises to 2.0 V and sometimes drops to 1.8 V. All other input voltages, and the voltages the component produces are normal.
my device setup is as follows:
VDD_33_AUX not used and pulled down using a 10K resistor.
GRST floating.
We tried to improve the soldering, but it did not help.
Please Advise,
Regards,
Yossy Goldenberg