Hi Team,
Does DS90UB936 support two channels of 1080P30 (YUV422) video access at the same time? Is the bandwidth enough?
In addition, do the two videos have to be frame synchronized or can they be out of sync?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Does DS90UB936 support two channels of 1080P30 (YUV422) video access at the same time? Is the bandwidth enough?
In addition, do the two videos have to be frame synchronized or can they be out of sync?
Hello Amelie,
yes, it should be supported.
It does not matter if they are synchronized or not. This depends on the selected Port forwarding mode. For more details on this, please refer to the d/s, section "7.4.28 CSI-2 Forwarding"