This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750EVM: Is it possible to import configuration from a current device (TPS25750)?

Guru 29720 points
Part Number: TPS25750EVM
Other Parts Discussed in Thread: TPS25750,

Hi Team,

My customer bought TPS25750EVM and using TPS25750 application customization tool.
He asked the following.

1)
Is it possible to import configuration from a current device (TPS25750)?

2)
Is there a default configuration image of TPS25750EVM?
I would just like to know if we can recover the configuration image that is flashed at the time of shipment.

Best Regards,
Yaita

  • Yaita,

    1. Currently it is not possible to export the configuration from a device back into the GUI
    2. I have requested the default configuration image for the TPS25750EVM be placed on an E2E FAQ. This will likely take the form of a JSON file that is importable into the Web GUI. Once this is complete, we'll update this ticket with a link to that post.