Other Parts Discussed in Thread: TLK2711-SP
First thanks for the answers to questions already posted about the TLK2711 - a great help. I have some other questions.
1. What does the TLK2711 transmit when an invalid K-code is entered into the TXD[15:0] inputs with TKLSB and or TKMSB set high indicating a K-code. For example what will it send when K15.0 is entered i.e. TXD[7:0] = 000 01111 and TKLSB is 1.
2. It is unclear what the receiver will do when it receives a comma with negative disparity. The TLK2711-SP data sheet states that the data corresponding to the comma codes should only be present on RXD[15:8] or RXD[7:0] when the comma code has positive disparity, i.e. previous running disparity is negative, see note under Table 4 “(1) Should only be present on RXD0-RXD7 when in running disparity <0". It does not mention what is present on RXD[15:8] or RXD[7:0] when the comma code has negative disparity (i.e. previous running disparity is positive). I assume that this note is misleading and that the K28.1, K28.5 and K28.7 code will appear on the output of the receiver, regardless of the previous running disparity. It is only symbol synchronisation that will not occur if one of these three codes is received with negative disparity (previous running disparity positive).
3. The data sheet states on page 9 just above table 3, “An error detected on either byte, including K codes not in table 4, causes that byte only to indicate a K.0.0 code on the RKxSB and associated data pins, where K0.0 is known to be an invalid 8B/10B code. What other errors are detected? Is it just invalid K codes, or are invalid running disparities reported i.e. running disparity in the receiver is something other than +1 or -1? Are there any other receiver errors that are detected?
4. Referring to the Power-Down Mode on Page 10. Can you confirm that RKMSB is not tri-stated in the Power-Down mode? Is the shutdown current of 3 mA (in the Electrical Characteristics Table) with the TXCLK signal active? If not, what is the shutdown current when TXCLK is active (TXCLK need to be active to perform signal detection in power-down mode)?
5. When PRBSEN =1, what appears on the RXD[15:0] and RKMSB signals? RKLSB is used to monitor the results of the PRBS test.
Thanks for your help.