Part Number: SN65HVD1781
Other Parts Discussed in Thread: TMUX1237, TMUX1119, TMUX1219
Hello,
I have to use common hardware circuit with SN65HVD1781 transceiver for both J1708 and RS485 interface with software change if required. I can make two assembly variant with minor component change, but not with transceiver part number change. There is a possibility of inversing the signal of UART Tx for DE in case of J1708 application. But my worry is Tx should be connected to D for RS485 and inversed Tx should be connected to DE, D should be grounded in J1708. How can I implement this two options in common circuit?
Please support
Regards,
Ganesh