Other Parts Discussed in Thread: TCAN4550, MSP430FR6989
Hi all,
I currently have a S32K148EVB dev kit and a TCAN4550EVM. I want to be able to use the CAN board as an additional bus on the dev kit (Chip can support 3). I have connected the two boards as follows:
| S32K148EVB | TCAN4550EVM |
| MOSI | SDI |
| MISO | SDO |
| SPI Chip select | nCS |
| SCLK | SCLK |
| 5v (10k resistor) | Reset |
Firstly does this seem correct?
Secondly is there any example code for the low level SPI driver with this master board? Its a small part of my project and something I have never done before so all and any help is greatly appreciated!
Also, if this is a question more suited to the NXP side of help then I will go that way, thanks!