Part Number: DS90UB962-Q1
Can we use UB962 to replace UB960? We use only MIPI CSI0 of UB960.
Is the transfer speed of UB962 the same as UB960?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB962-Q1
Can we use UB962 to replace UB960? We use only MIPI CSI0 of UB960.
Is the transfer speed of UB962 the same as UB960?
Thanks.
Hello Hui-Liu,
Yes, you can use it to replace the 960 if your input data rate is not higher than 3Gbps.
Note: the UB960 supports data rate of 4Gbps
Theoriticaly yes, but as you can see in the datasheet, the UB964 is Compatible With DS90UB913AQ/913Q/933Q Serializers