Part Number: TPS25750
Hi,
I was using the GUI to get the binary file for this device and noticed that i cannot configure GPIO12 as the "alternative function I2Cm_IRQ". When i click on GPIO11 though, i am able to set it as this alternate function. Since this is different from the datasheet, how can i set this up? Also, i noticed there is a Low Region Binary button in the generation options. What does this format do exactly as i noticed it is about half the size of the Full flash binary?
Thanks,
Jose