Part Number: TCA9802
Please help confirm the following problems about tca9802
1. for the following functions of tca980xb side current source, when vccb is low, current source disable.
(1) Vccb is low. What should vccb do? Floating or resistance to GND? How does "week pull up is connected with back power protection" understand?
(2) When B-side current source is disabled, can sclb/sdab be connected with pull-up resistance to external power supply for level shift?

2.How to understand iilc minimum 1000ua ? If the tca980x is to transmit low current, the B side device must sing at least 1000ua current, and the corresponding RILC is 150 ohm? If the RILC is less than 150 ohm, the B side needs to sing more current to output low?
![]()
thank a lot
john