Hi Team,
Customer planned to use USB3 Mux HD3SS3212.
When customer started the layout, customer found that the layout trace of Mux and the connector side are staggered. So can customer swap the USB3 Tx polarity as this picture ?
ASIC Tx+ connect to Mux pin4, and Tx- connect to pin3. Also the same swap at connector side pin 18,19 and pin 13,14. This swap will cause layout trace smoothly,
here is the schematic download link.
https://txn.box.com/s/rc2vg9rpp9mzb3n11pykni38zosul5p0
BR,
SHH