Part Number: DS90UB948-Q1
Hi team,
one question, what' the init sequence between 947 and 948? are they independent or 947 need to follow 948?
which one should be init first? thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Hi team,
one question, what' the init sequence between 947 and 948? are they independent or 947 need to follow 948?
which one should be init first? thank you
Hi Betty,
You need to follow the 947 init sequence on datasheet first and then init 948.
The 948 should also be powered up after a compatible Serializer has started sending valid video data. If this condition is not satisfied, then a digital (software) reset or hard reset (toggling PDB pin) is required after receiving the input data.
Best Regards,
Charley Cai