Part Number: TUSB8041
Other Parts Discussed in Thread: TUSB542
Customer is experiencing some issues with the TUSB8041.
1. During power-cycle test, the USB3.0 HUB is not properly recognized
2. During low-temperature startup test, there is leakage to 1.1V
Internal TI Drive Link to Detailed Issue Description
SBD of use-case is on p5, schematics on p6,7
The setup is Host - TUSB8041 #1 - TUSB8041 #2 - USB3 connectors
Abnormalities / summary of tests shown on p3
Waveforms on p4
Problem 1:
- During OFF/ON power-cycle test, about once every few-hundred times, the 2nd TUSB8041 hub doesn't get recognized
- 1st NG Issue: 2nd TUSB8041 HUB is not recognized by Host PC
- 2nd NG Issue: The 2nd TUSB8041 HUB identification fails, and the Host PC shows the Δ! mark
- 3rd NG Issues: Both the 1st/2nd TUSB8041 HUBs are not recognized by Host PC
For 1st / 3rd above, even when GRSTz was pulled to GND, the HUBs did not recover.
Are there any thoughts on to what could be causing this?
Problem 2:
- Under low-temperature power-on testing, before 1.1V rail is powered up, there seems to be 200mV of leakage on the line
- Due to the following, we believe this is leakage due to TUSB8041 HUB:
1) By removing the TUSB8041 HUB the condition resolves itself
2) Using a cooling-setup to specifically target only the TUSB8041 and cool it, causes the condition to occur
Are there any thoughts on to what could be causing this?
Other:
The setup doesn't use an EEPROM, and OTP is Default settings.
Reset is an Active Reset. Power is supplied 3.3V then 1.1V.
10ms after the 1.1V rises, Reset is released.
Regards,
Darren