Part Number: DP83822I
Hi team,
About DP83822, I have a few questions on LED configuration.
We target to implement mode2 as below:

Configure CRS:

Strap pins LED0/LED1 are both used default configuration without external pull up or pull down resistors:

I find description about LED in datasheet, but do not well understand it:


Then I should use the circuit for pull up for LED_0, and use circuit for pull down for LED_1, am I right? Is the LED_1 pin should be take as a pulled down pin? Does the parallel resistor for LED effect the strap result?
Best regards,
Wendy