This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1042I: Can our TUSB1042I replace PTN36241G+FUSB340TMX

Part Number: TUSB1042I


Hi team,

I want to check whether we have integrated solution to replace below devices? can TUSB1042I work?

for USB 3.1,(TYPE C 5Gbps)

PTN36241G:    USB data driver chip

FUSB340TMX:    USB data swich chip

PCMF1USB3SZ:   ESD protect

thanks.

  • Hi,

    Correct TUSB1042I can be used to replace FUSB340TMX and PTN36241G. TUSB1042I also supports Gen 2 operation. If customer is looking for Gen 1 only device TUSB542I can also be used. External ESD will still be needed with both devices.