Part Number: TPS65987D
Hi,
Is there any way to get the TPS interface chip to sleep with a USB-C cable connected? I'm open to external measures because I understand this is not the normal mode of operation.
We have a situation where an external battery pack will be plugged in and is supposed to provide many days of power. The possible scenario I could see is our micro wakes the TPS interface up when our internal battery gets low. At that point the TPS connects to the external battery, negotiates power, the system charges for a bit, and then is commanded back to sleep.
We would need to do this because the standby current for the external battery and for TPS chip are just too high.
Perhaps a FET on the Vbus line from the USB-C connector going into the TPS might achieve this?
C