Other Parts Discussed in Thread: TUSB4020BI, TUSB8020B
Hi, Support Team
There was a request for a recommendation for products that can be used with USB Hub from a customer.
The features of the product are as follows.
1. When connecting with host and USB, connect with two devices through Hub IC.
2. Connected to one of the two connected devices to communicate with the host
When implementing the above function, I would like to switch the two connected devices through the Vbus voltage.
A simple block diagram is attached.

If you have a USB HUB or Switch IC capable of implementing this function, please recommend it.
If there is a solution that can be implemented even if it is not one-chip, please recommend it.
Thanks.
Regards,
MJ