Part Number: DSLVDS1001
Other Parts Discussed in Thread: SN74AXCH1T45
Dear *,
we have to generate 100MHz clk from single ended clk to differential clk.
we came across DSLVS1001 and it has good LVDS output 1.25V ± 350mV but then input high voltage min is 2V and our CLK is 1V8.
So we have to convert CMOS 1.8V 100MHz clk to LVDS differential 100MHz clk with 1.2V ± 350mV, do you maybe have a solution for this kind of setup?
Or can we put something in front of DSLVS1001 to convert from CMOS to LVCMOS/LVTTL ?
Best Regards,
David.