Other Parts Discussed in Thread: BQ76952, TCAN1051
Hi, TI experts
I have a question about bq76952.REG2 LDO
The BQ76952 datasheet shows an example application where the REG2 LDO output is supplying 5V power to a CAN transceiver. However, the LDO output current limit of 45mA is too low to meet the supply current requirements of TI's TCAN1042 or TCAN1051 transceivers (80mA max in dominant mode, up to 180mA with the bus faulted).
Is there a recommended CAN transceiver which will not overload the REG2 output of the BQ76952?
Waitting for your comments.