Part Number: DS160PR410
Hello,
At page 20 at the datasheet of DS160PR410 there is a note regarding the AC-coupling capcitors of the DS160PR410:
* Place AC-coupling capacitors near to the receiver end of each channel segment to minimize reflections.
As I understand, that means that the AC-coupling capacitors should be placed near the receiver input.
This demand collides with the demand of the transmitter to put AC-coupling capacitors at the output of the transmitter.
1) Should I place AC- coupling capacitors at the output of the trasmitter and at the input of the receiver?
2) If not, where should I place the AC-coupling capacitors? At the input of the receiver or at the output of the transmitter?
Best regards,
Asaf Abraham