Part Number: TPS25858-Q1
Hi Team,
Can you please check and advise with following request?
What your alternative suggestions here?
"
We have examined your TPS25858-Q1 in order to evaluate it in our automotive project, whose features I have shared in the table below.
Considering the maximum values of the product, can a 24V system work continuously under 29V input voltage?
Maximum Ratings (For One Port Only) Vin = 9-29V, Io = 3A, Vo = 5V, Pmax = 15W
Nominal Ratings (For One Port Only) Vin = 12-24V, Io = 1.5A, Vo = 5V, P = 7.5W
"
Thanks in advance
Best Regards
Furkan Sefiloglu