Part Number: ESDS304
Other Parts Discussed in Thread: ADS8681
Hi there.
I'm using 3.3V 10MHz SPI signals in a design and need to protect them from transients.
I found the ESDS304DBVR and was wondering if it's suitable for my application.
The part (ADS8681) with the lowest tolerance along the path in this design has a maximum input voltage rating of 3.6V.
The ESDS304DBVR is rated @ Vrwm = 3.6V, Vbrf = 4.5-7.5V and Cline = 2.8pF max, though I'm not sure about Vclamp though. Is it suitable among the stated Ipp variations?
If not is there another suitable device that you can recommend or perhaps another technology?
Thanks,
Al.