Part Number: MAX3232
Hi,
my customer was using SP3232EEY, and I searched online that MAX3232E is the right choice to replace it.
But the supply of MAX3232E is not good and MAX3232 supply is good at the moment.
And the only difference is that MAX3232E has Contact Discharge and Air-Gap Discharge parameter but MAX3232 doesn't have.
Then I wonder what side effect if I use MAX3232 instead of MAX3232E in the application?