Part Number: TCA4311A
Dear TI Team
Data sheet Fig.12 is introduced as an example of a circuit for communication between one master and multiple slaves.
I have a question about this circuit example.

1. In this example, TCA4311A is placed on the slave side (I / O Peripheral Card side), but is TCA4311A used on the master side (Backplane side)?
2. If TCA4311A is not used on the master side of Fig. 12, the buffer is placed only on the slave side. At this time, is there a merit of arranging the TCA4311A only on the slave side as shown in Fig.12.
(Usually, I think that the buffer is also placed on the master side)
Best Regards,
Y.Ottey