This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET1151P: Is the LOS signal of ONET1151P too low power or signal LOS?Which register can be used for control?

Part Number: ONET1151P


Is the LOS signal of ONET1151P too low power or signal LOS?Which register can be used for control?

  • Greetings,

    LOS signal is asserted when signal level falls within certain threshold. 

    LOS event causes LOS pin to get activated. Through the register LOS pin assert level can programmed - if desired. In any case, LOS pin indicates loss of signal occurence.

    Regards,, nasser