This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953A-Q1: DS90UB953A-Q1

Part Number: DS90UB953A-Q1


Hi,

From DS90UB953A-Q1 datasheet, MIPI version is as follows

D-PHY v1.2 and CSI-2 v1.3 compliant system
interface

The system involves data sent to 953 serializer from xilinx mipi csi-2 tx subsystem ip 

xilinx mipi tx csi-2 subsystem ip mipi version is as follows

D-PHY v1.2 and CSI-2 v1.2

The CSI-2 version on 953 serializer is CSI-2 v1.3 and xilinx mipi tx ip is CSI-2 v1.2

Can these two be connected? Will there be any compatibility issues?

  • Hello Jay,

    The CSI-2 1v3 Specification leverages D-PHY 1.2 and introduces the C-PHY 1.0, both with improved skew tolerance and higher data rates. These enhancements enable higher interface bandwidth and more flexibility in channel layout. The CSI-2 1.3 Specification was designed to ensure interoperability with CSI-2 1.2 when the former uses the D-PHY physical layer.