Part Number: TUSB212
Other Parts Discussed in Thread: TUSB216I
Hi Expert,
Customer has connector to bridge CPU board and main board.
Here is the estimate layout of USB trace
CPU <=6inch=> SMT_CONN <=20inch=> USB_A_CONN
Refer to Intel design guide, trace length of “2 Connector Topology” recommend to less than 8 inch.
Intend to add TUSB212 to solve trace length issue,
Please suggest where is more proper to place TUSB212 or if recommend to have two TUSB212?
Two methods below we are thinking of and would like to have your advise. If you have other suggestions, please let us know.
- if the below location of TUSB212 OK?
CPU <=6inch=> SMT_CONN <=20inch=> TUSB212 <=1inch=>USB_A_CONN
- or if we could add 2x TUSB212 such like:
CPU <=6inch=> SMT_CONN <=2inch=> TUSB212 <=19inch=> TUSB212 <=1inch=>USB_A_CONN
Thanks,
Allan