Part Number: DP83822I
A question about boot ROM
Do the gpio37 and gpio34 have to be given a high level by the outside when the boot mode is mode 3? Can I enter boot mode 3 without high level? If not, is there a risk? What are the risks?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822I
A question about boot ROM
引导模式选择模式3,GPIO37和GPIO34必须由外部给个高电平么?不给高电平是否能进入引导模式3?如果不给高电平,是否有风险?有什么风险?
Do the gpio37 and gpio34 have to be given a high level by the outside when the boot mode is mode 3? Can I enter boot mode 3 without high level? If not, is there a risk? What are the risks?
Hi Zhang,
I am not sure I completely understand your question. There are no pins on the DP83822 called "gpio37" and "gpio34". Are you referring to the GPIO strap pins in general on the PHY? For the strap pins, if you want mode 3, then the voltage on those pins needs to be as specified for mode 3 in section 8.5.1 of the datasheet.
Regards,
Adrian Kam