Part Number: AM26C31
Hi,
My customer has the questions of AMC26C31 output. Please advise us.
- Datasheet said Vod (Differential output voltage magnitude) = 3.1V (Typ) on RL = 100ohm. This condition is Figure 2. On this condition, does this current flow on Vod/RL=31mA? Please let us know. Also, on this condition, are IOH, IOL over 20mA (Recommended operation condition Ioh/Iol)??
- Datasheet said Vod (Differential output voltage magnitude) = 3.1V (Typ) on RL = 100ohm. Is Vod depend on RL? For example, if RL is larger tham 100ohm, Vod(min) is smaller than 2V. Is it correct? Also, if RL is smaller tham 100ohm, Vod(min) is larger than 2V. Is it correct?
- Which is influence of Vod variation, depend on lot variation or depend on temperature? Can TI provide the graph of Vod to understand trend of temperature?
- Can TI provide the graph/spec related with Vcc and Vod/Voh/Vol
Thanks and best regards,
M.HATTORI.