Part Number: TMDS181RGZEVM
Other Parts Discussed in Thread: TMDS181
Hello expert,
I have question for TDMS181EVM.
My customer start to evaluate TMDS181 using EVM.
Then, they want to know initial operation mode of TMDS181EVM when they only connect power source to EVM.
As far as I understand, I think default register setting is loaded.
So this device will be "Automatic redriver to retimer crossover at 1.0 Gbps (default)".
HDMI's data rate is higher than 1.0Gbps with all revision.
So I guess this device is work as retimer when they start to supply power for EVM.
Is this understanding correct?
Best regards,
Kazuki Kuramochi