Part Number: DP83848M
Hi Team, seeking your assistance from a customer. Attached is the schematic.
The main concerns are.
If the clock reference is correct with the RMII mode.
Do I need to use 25MHz or 50MHz in X1/X0 pin using RMII mode?
Should I connect a 50MHz reference signal between the PHY and the micro? If yes, which on PHY's pin should be used?
Thank you.
-Mark