Part Number: DP83867IS
The DS specifies there are no power sequence timing requirements when in Two-Supply Mode.
Q1: Should device be held in reset until both power rails come up?
Q2: in Two-Supply mode (2.5V and 1.1V) the CLK still needs to be a 1.8V signal, yes?
Q3: Is there a timing requirement for CLK? Can 1.8V CLK be applied before 2.5V, etc...
Q4: Should device be held in reset until both power rails, and CLK are all up?
EDIT: For Q3/Q4 above, if device needs to be held in reset until supply rails and CLK are up, how long after CLK is supplied before device can safely be released from reset? What if device reset is released on a CLK edge, etc?