Part Number: TPS25750EVM
Other Parts Discussed in Thread: TPA3255EVM, TPS25750
Hello,
I have purchased the TPS25750EVM and just received it today. I tried to flash the settings using the online/offline application, but I wasn't able to flash the device using any of the apps.
My offline app indicates that the hardware is connected to the device through a COM9 port, but when I try to flash it, it gives me an error saying power cycling is needed for the board.
I just connected my board using a regular micro USB cable and I haven't changed any jumpers. I'm trying to use the TPS25750EVM to power TPA3255EVM, but I'm stuck at step 1.
Is there any setting that I could have missed out? I'm not using any USB hubs from my computer. The micro USB cable is directly connected from my desktop's mainboard USB 2.0 port.
Also, I have an additional question about powering my AMP EVM. If I connect 20V/5A USB PD power supply using USB C, Should I jump wires from the PPHV pins to my audio AMP board?