Part Number: SN65HVD35
Hi,
Could you let me know maximum nodes of SN65HVD35 for RS-422?
At 1/8 UL, 8*10=80 nodes. is it correct?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD35
Hi,
Could you let me know maximum nodes of SN65HVD35 for RS-422?
At 1/8 UL, 8*10=80 nodes. is it correct?
Thanks.
Hi David,
If we're purely discussing what the RS-422 standard will allow, this would be correct. However, if we were to use the same hardware for the system and define it as a RS-485 network, this standard would allow 256 nodes. The reason for this is how the two standards define the maximum number of allowable nodes. Where RS-422 states that 10 receivers of a specified input resistance may be used on one bus, the RS-485 standard defines the unit load (U.L.) term based on a different input resistance value and allows 32 of these U.L.s.
A good depiction of these differences is shown in table 4 of this application report.
Let me know if you have any questions about this.
Regards,
Eric Schott.