Part Number: DS250DF410
Hello all,
I'm developing camera sensor hardware.
developing camera sensor is too high resolution sensor (24MP) to transmit with serdes.
so I'm interested in long transmission data within mipi- csi2 protocol .
Is DS250DF410 possible to transmitte mipi csi-2 protcol?
my camera device specification is as shown below.
mipi- csi2 v1.2
D-phy 4 lane
data rate 2043Mbps / lane.
resolution : 5760 x 4312 pixel
could you recommended how to transmit mipi csi2 protocol over 6 meter?
thanks,