This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Can meet my customer's requirements?

Part Number: DP83867IS


Hello

My customer is thinking of DP83867IS for their new design.
But, they are not sure if DP83867IS can fully meets their following requirements 1) to 4).
Please let them know if DP83867IS is the right device or not. If DP83867IS is the right device, then please also let them know the required register setting to achieve 1) to 4) below.

  1. No auto-negotiation. Either fixed 10BASE-te or fixed 100BASE-TX.
  2. RGMII interface.
  3. To support “Link Fault Pass Through”, they would like to disable TX somehow.
  4. Monitor Link Status, and light an LED when a link is establish and brink it during data TX/RX activities.

Best regards,

K.Hirano