Part Number: HD3SS3212
The datasheet seems to jump around regarding which side of the MUX should have the AC caps on the SSTX lines.
Figure 7 shows the caps between the MUX and a USB-C connector to support flipping.
But then Fig. 8 and 11 turn around and show the caps between the device and the MUX, not between the MUX and connector.
Is there any affect on the EYE diagram with having the caps in one configuration vs the other?
I understand having caps on both sides means we need a biasing voltage - but if caps are only on one side of the MUX, which side is best, and why?
Darren