This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: About R1 and R2 of USB_VBUS

Guru 21045 points
Part Number: TUSB4020BI


Hi Team,

 

I understand that the role of USB_VBUS is USB upstream port power monitor and your recommended values are R1= 90.9kΩ ±1%, R2= 10kΩ ±1%.

However, I would like to change R1 and R2 values from your recommended values to R1=909Ω, R2=100Ω.

 

I guess that If USB_VBUS voltage is within the recommended range(0V to 1.155V), R1 and R2 can be changed.

-If R1=90.9kΩ and R2=10kΩ, USB_VBUS voltage is 0.495V

-If R1=909Ω and R2=100Ω, USB_VBUS voltage is 0.495V

 

Is my understanding correct?

If No, could you please let us know reason and any concern?

(For example; if R1 and R2 values are small, abnormal operation occurs etc.)

 

Regards,

Hide