This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCAN921224: lower data rate ser-des / clock synchronizer

Genius 17455 points

Part Number: SCAN921224
Other Parts Discussed in Thread: SN65LV1023A

Hi all

My customer has an application as illustrated in the below schematic where they are transferring data and an independent clock at 60MHz over a serial interface.

They might implement this with a ser-des like the SCAN921224, however these devices have a lower data rate limit of 100Mbps as they will multiply the clock (e.g. 10MHz) by a factor of 10.

Do we have a device that can support lower data rate ?

Or do we have a PLL that can be used as the block indicated with "?" and that could regenerate the clock from the data stream  ?

Best regards

Ueli