Part Number: DS90UB953-Q1
Dear All
I would like to understand what are the limitations of the TI953/TI954 serdes when pairing with an Image sensor.
Inside the serdes datasheet, I am seeing 2 mains limitations:
- 4 Data Lanes at 832 Mbps Per Each lane
- Pixel clock = 100Mhz max for raw images
How can I integrate these 2 limitations if I want to run a sensor with 10M pixel, 30fps, 10bit output, 4 lanes, 25Mhz input clock for the image sensor?
Are there other limitations that should be taken into account?
Best,
Muriel