Part Number: DS90UB941AS-Q1
Hello ,
What would be the frequency for External reference clock input pin if the resolution is 960x430 .
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Hello ,
What would be the frequency for External reference clock input pin if the resolution is 960x430 .
Thanks
Hi,
Your PCLK must be above 25 MHz and you can either use the DSI CLK instead of a refrence clk or you can use a Oscillator that is connected to REFCLK0 that is the same frequency as the PCLK.
Regards,
Michael W.
Hi Michael,
Low jitter clock source to be used as external reference clock source as per datasheet , but No Jitter requirement in the datasheet .
your comments on this also please.
Thanks
,