Part Number: DS90UB960-Q1
Hi Team,
Is there a sample initialization sequence you can provide for the 960? Which registers are required to be configured for the 960 to work with 933 serializers?
Thank you,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Hi Team,
Is there a sample initialization sequence you can provide for the 960? Which registers are required to be configured for the 960 to work with 933 serializers?
Thank you,
Jared
Hello Jared,
if you configure the 960 Hardware correctly; i.e. MODE pin and PoC filter, then you will need only to change the back channel speed from 50Mbps to 2.5Mbps in register 0x58