Other Parts Discussed in Thread: TPS2071
Hi,
I would like to inquire that whether the assertion on reset pin is integral for boot up sequence of the IC or not? can the pin be left always as logic 1? my board is getting direct 3.3V supply and hence it diminishes any requirement of an LDO based USB Power Controller ICs (tps2071....5). The literature I went through suggest to not assert the pin until 90% 3.3 V is produced but in my case I have no such considerations since I am getting solid 3.3V externally.
Thanks,
Safi