Part Number: TPS65987DDK
Other Parts Discussed in Thread: TIDA-050014
Hi,
I am designing a device which is a pure power Sink. I want to use the TPS65987DDK as a PD controller to negotiate 20V 5A with a USB PD supply/source on the other end, but my device does not need to/should not ever act as a source for other devices. It has no onboard battery and will be powered only from the singular USB-C PD port.
With this in mind, is it still necessary to provide 5v to PP_CABLE? If so, what is the best option to do so?... regulated from VBUS seems awkward or not feasible. Either CC1 or CC2 will be VCONN input but we don't know which because of orientation.
Thanks,
Gray