Part Number: DP83TG720S-Q1
Hi team,
I don't see in the latest data sheet of the PHY DP83TG720S-Q1 anything about the SFD 1588 compliance . How can we use it ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TG720S-Q1
Hi team,
I don't see in the latest data sheet of the PHY DP83TG720S-Q1 anything about the SFD 1588 compliance . How can we use it ?
Hello Mr Basset,
720S does not support start of frame detect. Though latency numbers are low (as described in datasheet) and that can enable 1588 time stamping in the processors/MAC.
--
Regards,
Vikram
Hello Vikram,
So the anwer of Justin Lazaruc in an other topic of the forum about IEEE 1588 compliance "The DP83TG720 supports the 1588 SFD pulses but not the entire standard" means in fact that low latency of the PHY helps to have an accurate time stamping even if it's done at the MAC level ?
May be I have missed something in the data sheet, but there is only the maximum values for the latency time, what is the min value or the accuraty of this latency ?
One other question, do we have to be in "RS-FEC bypas mode" to optimize the latency jitter ?
Regards,
Didier.
Hell Didler,
Team is looking at the data to share the latency variation with you. And yes we have RS-FEC bypass mode as mentioned in the latency section in the datasheet on ti.com
--
Regards,
Vikram
Hello Didler,
It took a while to work with team to find the required latency variation you were looking for. In the current datasheet, we have put the worst case number + extra margin. But we understand that you and some other customers are also looking at variation of latency and not just the worst case number. So to highlight the variation in the latency, following are the numbers with extra guard band removed from max and min numbers added to the table :
| Receive latency | min | typ | max | Units | typ | |
| rgmii default | 6.308 | 6.324 | 6.34 | us | 6.324 | |
| rgmii with FEC bypass | 298 | 314 | 330 | ns | 314 | |
| sgmii default | 6.354 | 6.37 | 6.386 | us | 6.37 | |
| sgmii with FEC bypass | 343.5 | 359.5 | 375.5 | ns | 359.5 | |
| Transmit latency | ||||||
| rgmii default | 0.561 | 0.577 | 0.593 | us | 0.577 | |
| rgmii with FEC bypass | 561 | 577 | 593 | ns | 577 | |
| sgmii default | 0.618 | 0.634 | 0.65 | us | 0.634 | |
| sgmii with FEC bypass | 625 | 641 | 657 | ns |
641 |
We are doing some extra silicon characterization and will update the datasheet.
--
Regards,
Vikram