Part Number: SN65DSI86-Q1
Where to use this GPIO 4?
what happens when GPIO4 is pulled up and pulled down?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI86-Q1
Where to use this GPIO 4?
what happens when GPIO4 is pulled up and pulled down?
Hi,
GPIO4 by default is input, but can be configured through the register to be pulse width modulation (PWM) controlling the brightness of eDP display.
Unused GPIO needs to be pulled down or tied to GND.
Thanks
David
Hi,
Is GPIO4 being programmed as an input? If this is the case, then there is no function associated with GPIO4 being pulled high or low.
Thanks
David